Keysight 89600 VSA .NET API
Measurement Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Measurement Class


Glossary Item Box

This class provides the members required to configure and control a measurement.

Object Model

Measurement ClassAnalysis ClassAnalysisChannelCollection ClassAnalysisChannel ClassFrequencyVersusTime ClassTimeVersusTime ClassAverage ClassCorrectionSetup ClassNoiseCorrection ClassIQNoiseCorrection ClassCorrectionCollection ClassCorrection ClassDataRegister ClassCustomStepCollection ClassICustomStep InterfaceMeasurementData ClassMeasurementData ClassICustomStep InterfaceMeasurementData ClassMeasurementData ClassFrequency ClassFrequencyChannelCollection ClassFrequencyChannel ClassInput ClassAnalog ClassAnalogChannelCollection ClassInputArmingTrigger ClassDigital ClassDigitalChannelCollection ClassInputExtensionCollection ClassInputExtension ClassInputLogicalChannelCollection ClassInputLogicalChannel ClassInputMeasurementChannelCollection ClassInputLogicalChannel ClassRecording ClassPlayChannelCollection ClassPlaybackTrigger ClassSwitch ClassHardwareConfiguration ClassInputTrigger ClassInputTriggerChannelCollection ClassFrequencyMaskTrigger ClassInputCorrectionCollection ClassInputCorrection ClassCalibrationFileCollection ClassMeasurementData ClassStateDictionary ClassIMeasurementExtension InterfaceMode ClassIChangeGroup InterfaceProcessingExtensionCollection ClassProcessingExtension ClassHardwareConfiguration ClassCalibration ClassHardwareGroupCollection ClassHardwareGroup ClassHardwareGroup ClassInstrumentId StructureSpectrum ClassSpectrumFrequency ClassSpectrumFrequencyChannelCollection ClassInputGate ClassInputGateChannelCollection ClassSpectrumTrigger ClassStatus ClassTime ClassTimeChannelCollection ClassTimeChannel ClassUserCorrection ClassPlaybackUserCorrection ClassPlaybackUserCorrectionChannelCollection ClassPlaybackUserCorrectionLogicalChannelCollection ClassStatus Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Measurement 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class Measurement abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also