Keysight 89600 VSA .NET API
FbmcSettings Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : FbmcSettings Property


Glossary Item Box

Gets the FBMC settings object.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property FbmcSettings As FbmcSettings
C# 
public virtual FbmcSettings FbmcSettings {get;}
C++/CLI 
public:
virtual property FbmcSettings^ FbmcSettings {
   FbmcSettings^ get();
}

Remarks

This object is used only when ModulationScheme is set to ModulationScheme.Fbmc. If the version of VSA is too old to implement this, the property returns null.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also