Keysight 89600 VSA .NET API
GetCyclicSuffixPerSymbol Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : GetCyclicSuffixPerSymbol Method


Glossary Item Box

Gets the cyclic suffix guard interval of each OFDM symbol, as a fraction of the IFFT time length.

Syntax

Visual Basic (Declaration) 
Public Overridable Function GetCyclicSuffixPerSymbol() As Single()
C# 
public virtual float[] GetCyclicSuffixPerSymbol()
C++/CLI 
public:
virtual array<float>^ GetCyclicSuffixPerSymbol(); 

Return Value

An array containing the cyclic suffix guard interval of each OFDM symbol

Remarks

If the end of the array is reached, processing loops back to the symbol number specified by GuardIntervalRepeatIndex.

When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored, because FBMC does not use a cyclic suffix.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also