Keysight 89600 VSA .NET API
SetGuardIntervalPerSymbol Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : SetGuardIntervalPerSymbol Method


value
An array containing the cyclic prefix guard interval of each OFDM symbol

Glossary Item Box

Sets the cyclic prefix guard interval of each OFDM symbol, as a fraction of the IFFT time length.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SetGuardIntervalPerSymbol( _
   ByVal ParamArray value() As Single _
) 
C# 
public virtual void SetGuardIntervalPerSymbol( 
   params float[] value
)
C++/CLI 
public:
virtual void SetGuardIntervalPerSymbol( 
   ... array<float>^ value
) 

Parameters

value
An array containing the cyclic prefix guard interval of each OFDM symbol

Remarks

If the size of the array is less than the result length, processing loops back to the symbol number specified by GuardIntervalRepeatIndex. The value of GuardInterval is always equal to the first element of the SetGuardIntervalPerSymbol array.

When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored, because FBMC does not use a cyclic prefix.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also