| Visual Basic (Declaration) | |
|---|---|
Public Overridable Function GetGuardIntervalPerSymbol() As Single() | |
| C# | |
|---|---|
public virtual float[] GetGuardIntervalPerSymbol() | |
| C++/CLI | |
|---|---|
public: virtual array<float>^ GetGuardIntervalPerSymbol(); | |
Return Value
An array containing the cyclic prefix guard interval of each OFDM symbolIf the size of the array is less than the result length, processing loops back to the symbol number specified by GuardIntervalRepeatIndex. The value of GuardInterval is always equal to the first element of the SetGuardIntervalPerSymbol array.
When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored, because FBMC does not use a cyclic prefix.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00