Keysight 89600 VSA .NET API
GetTimeGapPerSymbol Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : GetTimeGapPerSymbol Method


Glossary Item Box

Gets the time gap before each OFDM symbol, defined in samples at the OFDM system sample frequency.

Syntax

Visual Basic (Declaration) 
Public Overridable Function GetTimeGapPerSymbol() As Single()
C# 
public virtual float[] GetTimeGapPerSymbol()
C++/CLI 
public:
virtual array<float>^ GetTimeGapPerSymbol(); 

Return Value

The array specifying the time gap before each OFDM symbol, defined in samples at the OFDM system sample frequency.

Remarks

If the array is empty (the default) then there are no time gaps in the signal. If the end of the array is reached, processing loops back to the symbol number specified by TimeGapsRepeatIndex. This is an array of floating-point values, but currently the values are always rounded to the nearest OFDM FFT sample.

When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also