| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property InitialEqualizerMode As InitialEqualizerMode | |
| C# | |
|---|---|
public virtual InitialEqualizerMode InitialEqualizerMode {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property InitialEqualizerMode InitialEqualizerMode { InitialEqualizerMode get(); void set ( InitialEqualizerMode value); } | |
Property Value
The default value is InitialEqualizerMode.Automatic.In Automatic mode the VSA tries to use any available information from known pilot and preamble subcarriers to estimate the initial channel equalizer. In Manual mode the user must specify which symbol index to use for constructing the initial channel equalizer. Symbol indexes start with 0 being the first symbol in the signal description. In both Automatic and Manual mode the equalizer is constructed using information from any known pilot and preamble subcarriers.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00