| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property MultipleAccessScheme As MultipleAccessScheme | |
| C# | |
|---|---|
public virtual MultipleAccessScheme MultipleAccessScheme {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property MultipleAccessScheme MultipleAccessScheme { MultipleAccessScheme get(); void set ( MultipleAccessScheme value); } | |
Property Value
The default value is MultipleAccessScheme.None.When set to MultipleAccessScheme.Scma, the properties in the ScmaSettings subclass can be used to control the SCMA demodulation.
When set to MultipleAccessScheme.Noma, the properties in the NomaSettings subclass can be used to control the NOMA demodulation.
SCMA and NOMA are not supported when the ModulationScheme is set to ModulationScheme.Fbmc.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00