| Visual Basic (Declaration) | |
|---|---|
Public Overridable ReadOnly Property NomaSettings As NomaSettings | |
| C# | |
|---|---|
public virtual NomaSettings NomaSettings {get;} | |
| C++/CLI | |
|---|---|
public: virtual property NomaSettings^ NomaSettings { NomaSettings^ get(); } | |
This object is used only when MultipleAccessScheme is set to MultipleAccessScheme.Noma. If the version of VSA is too old to implement this, the property returns null.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00