Keysight 89600 VSA .NET API
ReferenceConstellationValuesAutoDetected Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : ReferenceConstellationValuesAutoDetected Property


Glossary Item Box

Gets or sets a value indicating whether reference constellation values are auto-detected during demodulation, or manually specified via SetReferenceConstellationValues.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ReferenceConstellationValuesAutoDetected As Boolean
C# 
public virtual bool ReferenceConstellationValuesAutoDetected {get; set;}
C++/CLI 
public:
virtual property bool ReferenceConstellationValuesAutoDetected {
   bool get();
   void set (    bool value);
}

Remarks

When the signal has high SNR, auto-detection is reliable and this should be true. For low-SNR signals where auto-detection may fail, capture a high-SNR version of the same signal, call CopyAutoDetectedReferenceConstellationValuesToManualValues to save the auto-detected values (which also sets this to false) before measuring the low-SNR signal.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also