Keysight 89600 VSA .NET API
ScmaSettings Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : ScmaSettings Property


Glossary Item Box

Gets the SCMA settings object.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property ScmaSettings As ScmaSettings
C# 
public virtual ScmaSettings ScmaSettings {get;}
C++/CLI 
public:
virtual property ScmaSettings^ ScmaSettings {
   ScmaSettings^ get();
}

Remarks

This object is used only when MultipleAccessScheme is set to MultipleAccessScheme.Scma. If the version of VSA is too old to implement this, the property returns null.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also