| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property SynchronizationMode As SynchronizationMode | |
| C# | |
|---|---|
public abstract SynchronizationMode SynchronizationMode {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property SynchronizationMode SynchronizationMode { SynchronizationMode get(); void set ( SynchronizationMode value); } | |
Property Value
The default value is SynchronizationMode.TimeCorrelation.For signals with no preamble, SynchronizationMode.TimeCorrelation can be slow, so it is usually better to use SynchronizationMode.CyclicPrefix.
This property value is ignored and SynchronizationMode.TimeCorrelation is used if ModulationScheme is set to ModulationScheme.Fbmc.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)