Keysight 89600 VSA .NET API
TimeGaps Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : TimeGaps Property


Glossary Item Box

Gets or sets the time gap before each OFDM symbol, defined in samples at the OFDM system sample frequency.

Syntax

Visual Basic (Declaration) 
Public Overridable Property TimeGaps As Single()
C# 
public virtual float[] TimeGaps {get; set;}
C++/CLI 
public:
virtual property array<float>^ TimeGaps {
   array<float>^ get();
   void set (    array<float>^ value);
}

Property Value

The default value is an empty array. Each value in the array has a minimum value of 0.

Remarks

If the array is empty (the default) then there are no time gaps in the signal. If the end of the array is reached, processing loops back to the symbol number specified by TimeGapsRepeatIndex. This is an array of floating-point values, but currently the values are always rounded to the nearest OFDM FFT sample.

When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also