Keysight 89600 VSA .NET API
ReferenceFrequencyDefinition Enumeration
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : ReferenceFrequencyDefinition Enumeration


Glossary Item Box

Determines how the reference frequency of each ComponentCarrier is defined.

Syntax

Visual Basic (Declaration) 
Public Enum ReferenceFrequencyDefinition 
   Inherits System.Enum
C# 
public enum ReferenceFrequencyDefinition : System.Enum 
C++/CLI 
public enum class ReferenceFrequencyDefinition : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AssignedMeasurementChannelCenterThe reference frequency of a component carrier is the center of the first measurement channel assigned to it.—
ManuallySpecifiedThe reference frequency for all component carriers is manually specified via CarrierAggregation.ReferenceFrequency.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also