Keysight 89600 VSA .NET API
SynchronizationRegionSelection Enumeration
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : SynchronizationRegionSelection Enumeration


Glossary Item Box

Methods for selecting the synchronization region.

Syntax

Visual Basic (Declaration) 
Public Enum SynchronizationRegionSelection 
   Inherits System.Enum
C# 
public enum SynchronizationRegionSelection : System.Enum 
C++/CLI 
public enum class SynchronizationRegionSelection : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AutomaticSynchronization region uses up to the first 10 symbols of signal (after RF envelope search, if specified), and the full MeasurementExtension.SetResourceMap to define the reference signal.—
ManualSynchronization region is determined by the MeasurementExtension.SynchronizationReferenceInterval, MeasurementExtension.SynchronizationReferenceOffset, MeasurementExtension.SynchronizationSearchInterval, MeasurementExtension.SynchronizationSearchOffset properties.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.0

See Also