| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property EqualizerTraining As EqualizerTraining | |
| C# | |
|---|---|
public abstract EqualizerTraining EqualizerTraining {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property EqualizerTraining EqualizerTraining { EqualizerTraining get(); void set ( EqualizerTraining value); } | |
Property Value
The default value is EqualizerTraining.Pilots.When set to EqualizerTraining.Pilots, the OFDM equalizer is initialized ("trained") using the Pilots, Complementary Pilots
When set to EqualizerTraining.PilotsData, the OFDM equalizer is trained using the data subcarriers as well as pilots and complementary pilots.
The advantage of EqualizerTraining.PilotsData is it usually gives a more accurate estimate of the channel response, so it results in lower EVM. The advantage of EqualizerTraining.Pilots is that it is not affected by incorrect symbol decisions in the data (which can happen at lower SNR or or higher modulation orders).
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)