Keysight 89600 VSA .NET API
CustomTrigCommand Property
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.InfiniiVision Namespace > InputExtension Class : CustomTrigCommand Property


Glossary Item Box

Gets or sets a SCPI command to use for custom triggering on the oscilloscope.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property CustomTrigCommand As String
C# 
public abstract string CustomTrigCommand {get; set;}
C++/CLI 
public:
abstract property String^ CustomTrigCommand {
   String^ get();
   void set (    String^ value);
}

Remarks

This parameter is used to set trigger parameters on the oscilloscope that you cannot set directly from the Agilent.SA.Vsa.Trigger API. This parameter allows the user to take advantage of the Infiniium Series scopes extensive trigger conditioning and pattern capability.

You can enter a sequence of SCPI commands, beginning with ":TRIG" and separated by semicolons. The commands will be transmitted to the oscilloscope if CustomTrigType is set to true. The trigger style is overridden by the SCPI command specified with this property. SCPI Query commands are not supported.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also