Keysight 89600 VSA .NET API
Trigger Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Trigger Class


Glossary Item Box

Represents triggering of data for the measurement.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Trigger 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 

Remarks

The Trigger object represents the measurement data triggering functionality. Only one input channel can control triggering of the measurement. You can set the trigger level, hold off, delay, slope and the style of trigger. If the trigger style is free run, then all the other property values are ignored. There are two trigger objects, one for the hardware (Trigger) and one for the recording playback (Recording.Trigger).

Both the InputTrigger and PlaybackTrigger classes derive from this class. Therefore this base class may be used to control both the input and playback triggering for trigger functionality that is on this class in a polymorphic way.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also