Keysight 89600 VSA .NET API
SampleMode Property
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.InfiniiVision Namespace > InputExtension Class : SampleMode Property


Glossary Item Box

Gets or sets a value indicating what sample mode to use when acquiring data from the oscilloscope.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SampleMode As SampleMode
C# 
public abstract SampleMode SampleMode {get; set;}
C++/CLI 
public:
abstract property SampleMode SampleMode {
   SampleMode get();
   void set (    SampleMode value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also