Keysight 89600 VSA .NET API
RFInputPortControl Property
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace > InputExtensionChannel Class : RFInputPortControl Property


Glossary Item Box

Gets or sets the Rf input port to use.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property RFInputPortControl As RFInputPort
C# 
public abstract RFInputPort RFInputPortControl {get; set;}
C++/CLI 
public:
abstract property RFInputPort RFInputPortControl {
   RFInputPort get();
   void set (    RFInputPort value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also