Keysight 89600 VSA .NET API
Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace
See Also  Inheritance Hierarchy
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly : Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace

Glossary Item Box

The Agilent.SA.Vsa.HardwareExtensions.XSeries namespace contains classes and enums to control  any advanced input extension parameter for X-Series signal analyzers. 

Classes

 ClassDescription
ClassInputExtension Input Extensions for XSeries signal analyzers
ClassInputExtensionChannel Input extension channel for X-Series signal analyzer hardware extension.

Enumerations

 EnumerationDescription
EnumerationBitPacking Specifies the recording bit packing density of the XSeries analyzer
EnumerationDither The dither settings for XSeries instruments
EnumerationExtRefLockBW Specifies the bandwidth of the reference lock loop
EnumerationIFType Analog signal path settings for XSeries instruments
EnumerationInfluenceCriteria What to optimize for
EnumerationInstrumentUserCorrection Specifies how corrections defined in the instrument should be applied.
EnumerationLODither The LO dither on/off setting for XSeries instruments
EnumerationMixerMode The mixer mode normal/alternate setting for XSeries instruments. This switches the LO mixing mode from high-side to low-side and vice versa. This selection is not available with BBIQ or External Mixer inputs.
EnumerationPhaseNoiseOpt Specifies loop dynamics of the LO for different phase noise characteristics
EnumerationPreamplifier The PreAmp on/off setting for XSeries instruments
EnumerationRangeControl The RangeControl Auto/Manual setting for XSeries instruments
EnumerationReceiverCalibration Specifies how corrections that were created with the RCal (Receiver Calibration) instrument feature are applied to the acquired data.
EnumerationRFGainAdjustmentAllowed Specifies the RF Gain Adjustment Allowed state.
EnumerationRFInputPort Specifies the Rf input port
EnumerationTrigLocation Specifies the external trigger port to be used for the XSeries analyzer
EnumerationuWPath Specifies the signal path through the high band microwave circuits
EnumerationWidebandIFOutput The Wideband IF output on/off setting for XSeries instruments

See Also