Keysight 89600 VSA .NET API
GlitchFilterThreshold Property
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace > InputExtension Class : GlitchFilterThreshold Property


Glossary Item Box

Gets or sets the threshold to use for the glitch filter in ADC counts.

Syntax

Visual Basic (Declaration) 
Public Overridable Property GlitchFilterThreshold As Integer
C# 
public virtual int GlitchFilterThreshold {get; set;}
C++/CLI 
public:
virtual property int GlitchFilterThreshold {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 32.40

See Also