Gets or sets a value indicating whether the IF Path should be automatically determined based upon current span, trigger type, and segmented capture settings.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property IFPathAuto As Boolean |
| C# | |
|---|
public virtual bool IFPathAuto {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool IFPathAuto {
bool get();
void set ( bool value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 25.60
See Also