Keysight 89600 VSA .NET API
MeasurementInfluenceCriteria Property
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace > InputExtension Class : MeasurementInfluenceCriteria Property


Glossary Item Box

Gets or sets the measurement influence criteria to use (what criteria to use when influencing other parameters). The parameters that can be influenced by this parameter (when their associated Auto parameter is true) are: IFOffset.

Syntax

Visual Basic (Declaration) 
Public Overridable Property MeasurementInfluenceCriteria As InfluenceCriteria
C# 
public virtual InfluenceCriteria MeasurementInfluenceCriteria {get; set;}
C++/CLI 
public:
virtual property InfluenceCriteria MeasurementInfluenceCriteria {
   InfluenceCriteria get();
   void set (    InfluenceCriteria value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also