Gets or sets a value indicating whether the measurement influence criteria is automatically determined based upon the current type of measurement. When true then power spectrum based measurements will choose to use the
InfluenceCriteria.SpectralQuality criteria, otherwise the
InfluenceCriteria.Normal criteria will be used.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property MeasurementInfluenceCriteriaAuto As Boolean |
| C# | |
|---|
public virtual bool MeasurementInfluenceCriteriaAuto {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool MeasurementInfluenceCriteriaAuto {
bool get();
void set ( bool value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 27.00
See Also