Keysight 89600 VSA .NET API
MixerMode Enumeration
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace : MixerMode Enumeration


Glossary Item Box

The mixer mode normal/alternate setting for XSeries instruments. This switches the LO mixing mode from high-side to low-side and vice versa. This selection is not available with BBIQ or External Mixer inputs.

Syntax

Visual Basic (Declaration) 
Public Enum MixerMode 
   Inherits System.Enum
C# 
public enum MixerMode : System.Enum 
C++/CLI 
public enum class MixerMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AlternateMixer mode will be set to alternate state for X series instruments—
NormalMixer mode will be set to normal mixing mode for X series instruments—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.20

See Also