Keysight 89600 VSA .NET API
Preamplifier Enumeration
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace : Preamplifier Enumeration


Glossary Item Box

The PreAmp on/off setting for XSeries instruments

Syntax

Visual Basic (Declaration) 
Public Enum Preamplifier 
   Inherits System.Enum
C# 
public enum Preamplifier : System.Enum 
C++/CLI 
public enum class Preamplifier : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AdjustedNormal preamplifiers are in the Off state but the RF Gain has been adjusted30.25
HighGainEnable the high gain preamplifier.30.25
LowNoiseEnable only the low noise amplifier for X series instruments.25.60
LowNoiseAndPreamplifierEnable both the low noise amplifier and internal preamplifier for X series instruments. This is equivalent to On + LowNoise.25.60
OffPreamplifier will be set to the off state for X series instruments—
OnPreamplifier will be set to the on state for X series instruments which will turn on the internal low band and high band preamps when possible.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.20

See Also