Keysight 89600 VSA .NET API
ReceiverCalibration Enumeration
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace : ReceiverCalibration Enumeration


Glossary Item Box

Specifies how corrections that were created with the RCal (Receiver Calibration) instrument feature are applied to the acquired data.

Syntax

Visual Basic (Declaration) 
Public Enum ReceiverCalibration 
   Inherits System.Enum
C# 
public enum ReceiverCalibration : System.Enum 
C++/CLI 
public enum class ReceiverCalibration : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
CorrectionEach correction that is marked as Enabled in the instrument will be applied if possible.—
OffCorrections are not applied.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also