Keysight 89600 VSA .NET API
TrigLocation Enumeration
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace : TrigLocation Enumeration


Glossary Item Box

Specifies the external trigger port to be used for the XSeries analyzer

Syntax

Visual Basic (Declaration) 
Public Enum TrigLocation 
   Inherits System.Enum
C# 
public enum TrigLocation : System.Enum 
C++/CLI 
public enum class TrigLocation : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
PrecisionPrecision External Trigger25.60
Trig1Trigger1 In—
Trig2Trigger2 In—
Trig3Trigger3 In—
Trig4Trigger4 In31.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

The number of trigger ports available on the analyzer depends on the model

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.20

See Also