Keysight 89600 VSA .NET API
DCOffset Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Analog Class : DCOffset Property


Glossary Item Box

Gets or sets the DC Offset to be added to the input signal (normally prior to the ADC).

Syntax

Visual Basic (Declaration) 
Public Overridable Property DCOffset As Double
C# 
public virtual double DCOffset {get; set;}
C++/CLI 
public:
virtual property double DCOffset {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also