| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property Impedance As Double | |
| C# | |
|---|---|
public abstract double Impedance {get; set;} | |
Property Value
The impedance of the input channel. The default is 50 ohms unless the hardware is not capable of that. Setting the value causes the value to be set on all channels. Getting the value returns the value from the first channel.The ValidValues<T>("Impedance") method can be used to retrieve a list of valid impedances for the current hardware. When that method is used on this object it will return the valid values of impedance for the first channel.
For multi-channel hardware, Impedance can be set independently for each channel or all channels can be set to the same value. To set the Impedance for an individual channel, use the Impedance property on the appropriate channel. Individual channel settings are available via the Channels collection. To set the Impedance for all channels to the same value, set the value of this property. It will take care of iterating through all the channels and setting the same value for them.
When queried, this property always returns the value for the first channel. For multi-channel hardware, the Impedance for an individual channel can be retrieved via the Impedance property on the appropriate channel. Individual channel settings are available via the Channels collection.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)