| Overload | Description |
|---|---|
| Create() | This method returns a handle to the Application object of an already running instance of Keysight 89600 VSA software, if any. |
| Create(Boolean,String,String,Int32) | This method returns a handle to the Application object of an instance of Keysight 89600 VSA that is listening on the indicated port number on the indicated host, optionally creating an instance if requested. |
| Create(Boolean,String,String,Int32,Int32) | This method returns a handle to the Application object of an instance of Keysight 89600 VSA that is listening on the indicated port number on the indicated host, optionally creating an instance if requested and waiting for a stipulated period of time for the new instance to start. |
| Create(Boolean,String,String,Int32,Int32,CreateOptions) | This method returns a handle to the Application object of an instance of Keysight 89600 VSA that is listening on the indicated port number on the indicated host, optionally creating an instance if requested and waiting for a stipulated period of time for the new instance to start. |
| Create(Boolean,String,String,Int32,Int32,CreateOptions,String) | This method returns a handle to the Application object of an instance of Keysight 89600 VSA that is listening on the indicated port number on the indicated host, optionally creating an instance if requested and waiting for a stipulated period of time for the new instance to start. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)