Keysight 89600 VSA .NET API
ApplicationFactory Class Members
See Also  Methods 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : ApplicationFactory Class

Glossary Item Box

The following tables list the members exposed by ApplicationFactory.

Public Methods

 NameDescriptionMinimum SW Version
Public Methodstatic (Shared in Visual Basic)CreateOverloaded. This method returns a handle to the Application object of an already running instance of Keysight 89600 VSA software, if any.  —
Public Methodstatic (Shared in Visual Basic)GetAvailableVersionsReturns a list of currently installed versions of the Keysight 89600 VSA software. The returned values can be used as an argument to the Create method.  14.00
Public Methodstatic (Shared in Visual Basic)GetInstallPathThis method returns the local install path for the version of Keysight 89600 VSA software represented by the supplied Application object.  —
Public Methodstatic (Shared in Visual Basic)GetRunningInstancesThis function allows the caller to discover all currently running instances of the Keysight 89600 VSA software on the local machine.  —
Public Methodstatic (Shared in Visual Basic)GetVersionInfoGets the version information for the specified release name of the VSA software that is currently installed on the local system that this call is being made on.  29.40
Public Methodstatic (Shared in Visual Basic)GetVersionInfosGets the version information for the specified release name of the VSA software that are currently installed on the local system that this call is being made on.  29.40
Public Methodstatic (Shared in Visual Basic)TryGetVersionInfoGets the version information for the specified release name of the VSA software that is currently installed on the local system that this call is being made on.  29.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also