| Visual Basic (Declaration) | |
|---|---|
Public Shared Function GetRunningInstances() As ApplicationIdentifier() | |
| C# | |
|---|---|
public static ApplicationIdentifier[] GetRunningInstances() | |
| C++/CLI | |
|---|---|
public: static array<ApplicationIdentifier^>^ GetRunningInstances(); | |
Return Value
An array of ApplicationIdentifier objects, each identifying a running instance of the application. If no instances are currently running, an empty array is returned.Note that the information returned is correct at the time the call is made. The caller must treat the returned information with care since existing instances can exit and new instances can start at any time.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)