Gets the version information for the specified release name of the VSA software that are currently installed on the local system that this call is being made on.
Syntax
Parameters
- versionNames
- A list of the release names (version strings from the GetAvailableVersions method) to get the version information for.
Return Value
A dictionary (keyed by the release name version) of version information for each release name version that was specified.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 29.40
See Also