| Visual Basic (Declaration) | |
|---|---|
Public Overloads Overridable Sub RecallSetup( _ ByVal fileName As String, _ ByVal append As Boolean _ ) | |
Parameters
- fileName
- The name of the file to recall. Supported files include Keysight 89600 VSA Software setup files (.SETX extension) and Agilent 89601A setup files (.SET extension).
- append
- When 'true', the setup information in the specified file is appended to the existing setup. Otherwise, when 'false', the setup information in the file replaces the existing setup.
This method appends the setup information contained in the specified file to the existing setup if the append parameter is 'true'.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.00