Keysight 89600 VSA .NET API
RecallSetup Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Application Class : RecallSetup Method


Glossary Item Box

Recalls a VSA setup file the specified path, replacing the existing measurements.

Overload List

OverloadDescription
RecallSetup(String)Recalls a VSA setup file the specified path, replacing the existing measurements.  
RecallSetup(String,Boolean)Recalls a VSA setup file from disk, possibly appending the measurements to the existing set of measurements.  
RecallSetup(String,Boolean,Boolean)Recalls a VSA setup file from disk, possibly appending the measurements it contains to the existing set of measurements.  
RecallSetup(String,Boolean,Boolean,DataSourceValueToUse)Recalls a VSA setup file from disk, possibly appending the measurements it contains to the existing set of measurements.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also