Keysight 89600 VSA .NET API
Average Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Average Class


Glossary Item Box

The Average object provides access to the VSA's averaging features.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Average 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also