| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property CalibrationMessage As String | |
| C# | |
|---|---|
public abstract string CalibrationMessage {get;} | |
When a calibration has failed the message begins with "Err" and, when detail is available, is followed by ": " and the underlying error text (for example the per-alignment failure). This is how a calibration error is reported - including a background auto-calibration failure, which does not raise a dialog - so it can be read programmatically (it is also returned by the SCPI :CALibration:MESSage? query) or shown in the user interface.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)