Keysight 89600 VSA .NET API
Calibration Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Calibration Class

Glossary Item Box

The following tables list the members exposed by Calibration.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyCalibrationMessageGets information about the calibration status (for example "OK", "Needed", or "Err").  —
Public PropertyIsAutoCalibrateEnabledGets or sets a value indicating whether automatic calibration of the hardware is enabled.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLastCalibrationGets the date and time of last successful calibration  —
Public PropertyModeGets or sets the calibration mode, which controls the trade-off between measurement accuracy and how often and how intrusively the hardware should be calibrated (aligned).  31.00
Public PropertyModeAutoGets or sets a value indicating whether the calibration mode is chosen automatically by the hardware. When on, the hardware selects the mode itself and Mode reflects the chosen mode.  31.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodBeginCalibrationStarts a full calibration of the input hardware.  —
Public MethodBeginQuickCalibrationStarts a partial calibration of the input hardware.  —
Public MethodCalibratePerforms a full calibration of the input hardware.  —
Public MethodCancelCalibrationCancels a calibration that is currently in progress.  31.00
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodQuickCalibratePerforms a partial calibration of the input hardware.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also