Keysight 89600 VSA .NET API
CancelCalibration Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Calibration Class : CancelCalibration Method


Glossary Item Box

Cancels a calibration that is currently in progress.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub CancelCalibration() 
C# 
public virtual void CancelCalibration()
C++/CLI 
public:
virtual void CancelCalibration(); 

Remarks

Has no effect if no calibration is in progress or if the hardware does not support cancellation. Use IsSupported("CancelCalibration") to determine whether the connected hardware supports cancellation before offering it.

Throws if the hardware reports an error while cancelling; callers should handle the exception (for example, to display it) rather than assume the cancel always succeeds.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also