| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property CableIFLoss As Double | |
| C# | |
|---|---|
public abstract double CableIFLoss {get; set;} | |
The loss at the IF in the IF/LO cable can be compensated for with this property by entering the loss in dB for the cable.
The cable loss will depend on the IF frequency. The IF frequency varies depending on which IF path (signal path) the measurement is using. For best accuracy, characterize the cable's loss for the IF frequency or frequencies that will be used.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)