Keysight 89600 VSA .NET API
ExternalMixer Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : ExternalMixer Class

Glossary Item Box

The following tables list the members exposed by ExternalMixer.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAuxIfFrequencyGets or sets the IF frequency if the mixer path is set to Aux IF path  19.52
Public PropertyBiasGets or sets the bias source for use with an external mixer.  —
Public PropertyCableCorrectionGets or sets the correction applied for the cable connecting the external mixer to the analyzer  28.40
Public PropertyCableIFLossGets or sets the loss at the IF in the IF/LO cable.  —
Public PropertyInputAttenuationGets or sets input attenuation in dB when the mixer has an input attenuator  26.00
Public PropertyIsBiasEnabledGets or sets a value indicating whether the mixer bias is applied  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMixerPathGets or sets the mixer paths  19.52
Public PropertyMixerSelectionGets or sets the type or band of external mixer used.  —
Public PropertyModelGets the model for the smart mixer (USB mixer).  —
Public PropertySerialNumberGets the serial number for the smart mixer.  —
Public PropertySmartMixerConnectedGets a value indicating whether a smart mixer is currently connected.  —
Public PropertySubbandsGets the collection of ExternalMixerSubband objects representing the sub bands for the external mixer setup.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also