Keysight 89600 VSA .NET API
FrequencyChannel Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyChannel Class


Glossary Item Box

This class is for channelized frequency parameters.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class FrequencyChannel 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class FrequencyChannel abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Remarks

The channels represented by this class are logical channels, which may be combinations of multiple physical hardware channels.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also