Keysight 89600 VSA .NET API
FrequencyChannelCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyChannelCollection Class


Glossary Item Box

This collection contains the set of FrequencyChannel objects representing the frequency settings for each logical input channel.

Object Model

FrequencyChannelCollection ClassFrequencyChannel Class

Syntax

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also