Keysight 89600 VSA .NET API
InputSampleRate Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > FrequencyChannel Class : InputSampleRate Property


Glossary Item Box

Gets the sample rate of the data from the instrument.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property InputSampleRate As Double
C# 
public abstract double InputSampleRate {get;}
C++/CLI 
public:
abstract property double InputSampleRate {
   double get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also