Keysight 89600 VSA .NET API
FftSize Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > FrequencyMaskTrigger Class : FftSize Property


Glossary Item Box

Gets the size of the FFT used by the mask trigger.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property FftSize As Integer
C# 
public abstract int FftSize {get;}
C++/CLI 
public:
abstract property int FftSize {
   int get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also