Keysight 89600 VSA .NET API
FrequencyMaskTrigger Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyMaskTrigger Class

Glossary Item Box

The following tables list the members exposed by FrequencyMaskTrigger.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAmplitudeReferenceStyleGets or sets the reference style to use for mask amplitudes.  —
Public PropertyCriteriaGets or sets the criteria for when a trigger will occur for a given signal relative to the mask.  —
Public PropertyFftSizeGets the size of the FFT used by the mask trigger.  —
Public PropertyFrequencyReferenceStyleGets or sets the reference style to use for mask frequencies.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLowerAmplitudeOffsetGets or sets the lower mask amplitude offset from the current Analog.Range of the trigger channel.  —
Public PropertyLowerFrequencyOffsetGets or sets the lower mask frequency offset in Hz.  —
Public PropertyMaskToUseGets or sets which of the upper or lower masks to use.  —
Public PropertyResBWGets or sets the resolution bandwidth.  —
Public PropertyResBWModeGets or sets how the ResBW is controlled for the frequency mask trigger.  —
Public PropertyUpperAmplitudeOffsetGets or sets the upper mask amplitude offset from the current Analog.Range of the trigger channel.  —
Public PropertyUpperFrequencyOffsetGets or sets the upper mask frequency offset in Hz.  —
Public PropertyWindowGets or sets the window type to use.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetLowerMaskAmplitudesGets the lower mask amplitudes.  —
Public MethodGetLowerMaskFrequenciesGets the lower mask frequencies.  —
Public MethodGetUpperMaskAmplitudesGets the upper mask amplitudes.  —
Public MethodGetUpperMaskFrequenciesGets the upper mask frequencies.  —
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetLowerMaskSets the lower mask for the frequency mask trigger.  —
Public MethodSetUpperMaskSets the upper mask for the frequency mask trigger.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also