Keysight 89600 VSA .NET API
GetUpperMaskFrequencies Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > FrequencyMaskTrigger Class : GetUpperMaskFrequencies Method


Glossary Item Box

Gets the upper mask frequencies.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetUpperMaskFrequencies() As Double()
C# 
public abstract double[] GetUpperMaskFrequencies()
C++/CLI 
public:
abstract array<double>^ GetUpperMaskFrequencies(); 

Return Value

Returns the frequencies in Hz. See FrequencyReferenceStyle for more information about what the frequencies may be relative to.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also