| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property TimeStepAuto As Boolean | |
| C# | |
|---|---|
public abstract bool TimeStepAuto {get; set;} | |
This setting is a boolean used to determine if the TimeStep is automatically configured based on the measurement Span. If true, the TimeStep is automatically set such that the block overlap (%) = 90. If false, the P:Agilent.SA.Vsa.FrequencyVersusTimeChannel.TimeStep% must be manually configured. The default value is true.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)